FS26 sbc watchdog notification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FS26 sbc watchdog notification

899 次查看
Albatros
Contributor III

Hi, I am using Sbc_fs26_example project. I realized in the main of this project we do not reload the sbc wdg. I saw SbcWatchdogNotification and i think if i use this i will have to reload the watchdog periodically. But when i added i saw that inside of the function was empty. Is there any example about this which i can use?

0 项奖励
回复
2 回复数

506 次查看
jochengerster
NXP Employee
NXP Employee

Hi

the watchdog notification will optionally be call only when the wdg configuration changes, to allow to adapt any custom SW scheduler (triggering the wdg) to stay synchronized. The also included Wdg driver can take care of triggering the watchdog.

jochengerster_2-1724838499771.png

 

There is also example code in the integration manual of the SBC driver

jochengerster_1-1724838455255.png

 

 

FYI, the Watchdog refresh notification is called after each refresh, to optionally evaluate the flags

jochengerster_3-1724838533805.png

 

 

best regards

Jochen

0 项奖励
回复

887 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Emre,

I have forwarded your SW related question to our FS26 SW expert, he is going to answer you through the Case #0059551.

BR, Tomas

0 项奖励
回复