Hello.
Hi.
1: Do you have successfully upload this script to programmer tool? : YES
2: Do you have a look after connect with load on SW2/3 LDO1? : NO. But, in both cases (normal and abnormal) the measurement environment was the same.
1. It was not related to the load.
2.There was no problem with the input voltage.
3. OTP_LDO1_SEQ
When OTP_LDO1_SEQ is less than or equal to 230,whether SW2/3 abnormal? : YES
Do you ever use your script3 to do OTP then test again to verify? : It was not tested in OTP mode.
Hi WS
Do you have plan to use Blank PF8100 on your board ?
If you just emulate and test before use the OTP part, I recommend you just need to focus on the things happen after PWRON HIgh, if use OTP device, the thing will be same to the POWRON high after TBB write, we don't need to care about the TBB write process.
Do you mind to provide your project information?
BRs
jinyu