Core Power Down Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Core Power Down Issue

5,317 次查看
schougule01
Contributor I

I am facing issue while loading script in the debugger.

I am getting "Core Power Down" issue while try to load script.

Is there any way to turn ON the Core Power to UP.

Controller: S32K148core_powereed down.png

标记 (1)
0 项奖励
回复
5 回复数

5,294 次查看
schougule01
Contributor I

Hi,

@danielmartynekactually there is no issue in script as it works for other hardware.

0 项奖励
回复

5,283 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @schougule01,

Do you mean it works with other S32K148 MCUs?

Since I can't reproduce it, I would like to test you script on my side.

 

https://www2.lauterbach.com/pdf/error.pdf

danielmartynek_0-1678871528969.png

 

Is the VDD powered?

 

Regards,

Daniel

 

0 项奖励
回复

5,298 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @schougule01,

If the MCU powered, can you measure the VDD?

Can you please share the script?

 

Thanks,

BR, Daniel

0 项奖励
回复

5,274 次查看
rweiss
Contributor V

This error message usually means that the core's power domain in the SoC is not enabled. If the whole SoC is not powered, the error message would be "target power down" and the debugger would usually display "power down" in the status bar.

Detection of "Core Power Down" is not 100% reliable, depending on the SoC it could simply mean "could not communicate with core", with disabled power domain being the most typical reason.

Regards,
Reinhard

0 项奖励
回复

5,272 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @schougule01,

Can you catch it right after POR?

system.CPU S32K148
wait state.power()
system.attach

 

BR, Daniel

0 项奖励
回复