Confirmation of how to use the PCA9956B driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Confirmation of how to use the PCA9956B driver

2,525件の閲覧回数
m-kamijo
Contributor I

Although this PCA9956B driver can handle LED drive voltages up to 20v, for example, if one LED is connected to one pin and two series connections are connected to the other pin, it is possible to use a single unit and a single unit. Can you expect similar behavior for both series connections?
We will wait for the answer.

// LED spec //

Vf 2.0v

If 20mA

2019/06/20

I wonder if it was something like this?

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,316件の閲覧回数
m-kamijo
Contributor I

It was saved. Thank you very much.

0 件の賞賛
返信

2,315件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Could you please give me your application Block diagram ?

0 件の賞賛
返信

2,315件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

About your application block there is no problem!

0 件の賞賛
返信