CANNOT Flash Program to MPC5775B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CANNOT Flash Program to MPC5775B

1,687 Views
jim_duan
Contributor II

cannot flash to MPC5775BE-416DS daughter card!

"Warning: Device is not detected or may be censored. Please enter password in GDB server parameters with debug

configurations using the flag -uncensorpassword=n, then restart the debug session."

S32 Design Studio for Power Architecture   Version: 2.1    Build id: 190624

Labels (1)
0 Kudos
1 Reply

1,570 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I believe it the same issue as in the similar case you have submitted recently.

Could you possibly share the solution for possible readers of this thread? Thanks

0 Kudos