BCC PCB design - Isloated communication to BCC or isolated CAN?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BCC PCB design - Isloated communication to BCC or isolated CAN?

1,614件の閲覧回数
Poley
Contributor V

Hey,

 

I usually use The MC33771C or similar in a distributed system. I need to make a new board which only has 1 BCC but also has CAN output and other controls so will be using a S32K IC.

Which of these 2 options is the suggested route or does it not matter?

1 - Normal S32K circuitry and SBC for power from an external source. Connects to BCC through TPL and transformer isolation to cover cell isolation

or

2 - S32K is powered by a switching reg DCDC from the cells and the BCC is connected by SPI. CAN output will then be through a islolated CAN trasciever and the SBC enable would be through an opto-isolator. - This would have the highest current draw from the cells

 

Thanks in advacne! Any thoughts are helpful.

0 件の賞賛
返信
5 返答(返信)

1,590件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

Q:Which of these 2 options is the suggested route or does it not matter?

[GW]The first one.

0 件の賞賛
返信

1,579件の閲覧回数
Poley
Contributor V

Great, thank you!

Does this look ok for the on board TPL? Do I still need the diodes around the transformer? Thank you!

Poley_0-1725914648027.png

 

0 件の賞賛
返信

1,566件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Sure,you need these diodes for getting protection.

0 件の賞賛
返信

1,546件の閲覧回数
Poley
Contributor V

Great, thank you!

And lastly can I confirm that if I want to use LED's to show that balancing is active (1 LED per cell). So LED is off with no current draw from cell when balancing is off and LED is ON when BCC balancing is on:

Starting from Cell 1 here:

Poley_1-1726055947135.png

 


Upto Cell 14 here:

Poley_0-1726055901605.png

Thank you!

 

0 件の賞賛
返信

1,531件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can try this mode.

0 件の賞賛
返信