8200如何按照自己的输出电压配置输出?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8200如何按照自己的输出电压配置输出?

249 Views
yangk
Contributor I

参数 比较多如何下手,哪些需要设置,那些不需要设置?SWx phase configuration有什么用?都为0可以吗

0 Kudos
1 Reply

228 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello yangk,

I hope all is great with you. Thank you for using the NXP communities.

In this case, I do recommend reviewing a preprogrammed device and using it as a reference for your design.

For example, you may use the Configuration report for PF8200 OTP program ID: DE as a reference. The Table 2 shows the configuration summary.

 

Note that the programming is based on the MCU/MPU requirements. The PF8200 is intended to work with the i.MX8QM.

I hope this information helps.

Regards,

David

0 Kudos