esd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

esd

642 Views
smkalim
Contributor I
We are looking for the surge protector in unidirectional and bi-directional mode. Can you suggest the part from NXPs portfolio if it matches the technical specifications?
 
High speed protectors  are the TVS devices to form an extremely low let-through energy barrier to excessive voltages and currents during surge events which may cause damage to unprotected high-speed, low voltage drivers and receivers. components. 
 
They are used in multiple applications but we need a 10/100M ethernet application.
 
  • Current required for the device to go from operating state to protected state- 750mA
  • Series resistance-1.4Ohms
  • Chanel to channel resistance-0.03ohms max
  • Time for the device to go from normal operating state to current limiting state - 50ns
  • Peak impulse voltage withstand with duration less than 1 ms - 40V max
0 Kudos
Reply
2 Replies

611 Views
kurdt784
Contributor I

Hello,

For surge protection in a 10/100M Ethernet application, consider NXP's PESD3V3L1BA or PESD5V0S1BA series surge protectors. These devices offer bidirectional protection with low series resistance (1.4 ohms), minimal channel-to-channel resistance (0.03 ohms max), and fast response time to transition from normal operating state to current limiting state. With a peak impulse voltage ADPVantage withstand of up to 40V, they effectively safeguard against excessive voltages and currents during surge events, ensuring protection for high-speed, low-voltage drivers and receivers.

0 Kudos
Reply

616 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi smkalim

For the ESD discrete products had already transferred to Nexperia.

You can directly contact with them for getting support!!

Thanks!

0 Kudos
Reply