support for yocto 2.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

support for yocto 2.6

ソリューションへジャンプ
1,862件の閲覧回数
emintz
Contributor I

Hi,

Does NXP intend to support next Yocto releases for QoriQ P and T series ? I mean Linux SDK promotion for Yocto 2.6 THUD last release. 

Another question, what the roadmap for QorIQ based cpu for powerpc arch ? Does NXP switch to ARM for it next generation products?

Thanks

0 件の賞賛
返信
1 解決策
1,661件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP LSDK 18.09 Linux Kernel 4.9 and supports the following PowerPC platforms.

MPC8548CDS

P2020RDB

T1042D4RDB

T1042D4RDB-64B

Please refer to the following readme file https://github.com/qoriq-open-source/yocto-sdk to download this git repository from the GitHub.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,661件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP SDK 2.0-1703 supports the P2041RDB board. NXP LSDK does not support the P2041.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,661件の閲覧回数
emintz
Contributor I

Hi Pavel,

What about P2041RDB ?

0 件の賞賛
返信
1,662件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP LSDK 18.09 Linux Kernel 4.9 and supports the following PowerPC platforms.

MPC8548CDS

P2020RDB

T1042D4RDB

T1042D4RDB-64B

Please refer to the following readme file https://github.com/qoriq-open-source/yocto-sdk to download this git repository from the GitHub.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信