Hi,
I want to configure sgmii interface in p1022 based card from uboot. Could any suggest what all changes need to be done in order to enable so. By default etsec mode is enabled
The P1022ds u-boot provides SGMII connection automatically. See attached file. It is tsec driver from NXP SDK 1.9. Find the init_phy procedure in this file.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel
Thank you for the above information