Hi Pavel,
Thanks for the update, however the issue is resolved to the point that meets our requirement. The root cause is still under debugging.
Basically the target we have has two non-volatile storage device. 1. Serial Flash (SPI) for boot code (u-boot) 2. Parallel NAND flash for uImage, File system, dtb and user data.
On target power-up , reset command does work perfectly fine from u-boot prompt. It is only after kernel boot-up that reboot command was not working(failed to reboot the target).
On debugging it is found that after probing and subsequent partitioning of Serial Flash(SPI) during kernel boot-up , the reboot does not work. i.e. trigger of HRESET_REQ does not reboot the target. However , on removing the Serial Flash probing and partitioning entry in dts, the reboot command does work from the kernel prompt. Since we do not require the Serial Flash(SPI) other than just the boot code (u-boot), we can meet our requirement by using the NAND flash only.