"bitbake -c configure -f virtual/kernel"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

"bitbake -c configure -f virtual/kernel"

跳至解决方案
6,135 次查看
shashankreddyvu
Contributor I

when i execute the below command in my terminal during system builder process it is giving following error.

"bitbake -c configure -f virtual/kernel"

NOTE: Psyco JIT Compiler (http://psyco.sf.net) not available. Install it to increase performance.

NOTE: Handling BitBake files: \ (0405/0405) [100 %]

Parsing of 405 .bb files complete (399 cached, 6 parsed). 536 targets, 1 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

NOTE: Preparing runqueue

NOTE: Executing runqueue

NOTE: Running task 248 of 248 (ID: 6, /home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb, do_configure)

NOTE: package linux-3.0.6-r1: task do_configure: Started

NOTE: package linux-3.0.6-r1: task do_configure: Succeeded

NOTE: Tasks Summary: Attempted 248 tasks of which 247 didn't need to be rerun and 0 failed.

mistral@mistral-veriton-series:~/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder$ bitbake -c menuconfig virtual/kernel

NOTE: Psyco JIT Compiler (http://psyco.sf.net) not available. Install it to increase performance.

NOTE: Handling BitBake files: \ (0405/0405) [100 %]

Parsing of 405 .bb files complete (399 cached, 6 parsed). 536 targets, 1 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

NOTE: Preparing runqueue

NOTE: Executing runqueue

NOTE: Running task 249 of 249 (ID: 7, /home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb, do_menuconfig)

ERROR: TaskFailed event exception, aborting

ERROR: Build of /home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb do_menuconfig failed

ERROR: Task 7 (/home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb, do_menuconfig) failed with 256

ERROR: '/home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb' failed

NOTE: package linux-3.0.6-r1: task do_menuconfig: Started

ERROR: Function do_menuconfig failed

NOTE: Task failed: ('function do_menuconfig failed', '/home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/build_p2041rdb_release/work/p2041rdb-linux/linux-3.0.6-r1/temp/log.do_menuconfig.3470')

ERROR: Logfile of failure stored in: /home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/build_p2041rdb_release/work/p2041rdb-linux/linux-3.0.6-r1/temp/log.do_menuconfig.3470

Log data follows:

|

| (gnome-terminal:3475): GLib-GIO-ERROR **: No GSettings schemas are installed on the system

| /home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/build_p2041rdb_release/work/p2041rdb-linux/linux-3.0.6-r1/temp/run.do_menuconfig.3470: line 484:  3475 Trace/breakpoint trap   (core dumped) gnome-terminal --disable-factory -t "$TERMWINDOWTITLE" -x $SHELLCMDS

| ERROR: Function do_menuconfig failed

NOTE: package linux-3.0.6-r1: task do_menuconfig: Failed

ERROR: TaskFailed event exception, aborting

ERROR: Build of /home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb do_menuconfig failed

ERROR: Task 7 (/home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb, do_menuconfig) failed with 256

ERROR: '/home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb' failed

ERROR: '/home/mistral/shashank/Material/FREESCALE_BACKUP/CD/installed/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-sdk-common-dpaa/recipes/linux/linux_3.0.6.bb' failed


please tell me how to sovle this problem and go to next step


Thank you.

标签 (1)
0 项奖励
回复
1 解答
4,737 次查看
mattsm
Contributor III

With system builder I think you need to look at setting TERMCMD and TERMCMDRUN to acceptable values. Your gnome-terminal looks broken.

在原帖中查看解决方案

0 项奖励
回复
10 回复数
4,738 次查看
mattsm
Contributor III

With system builder I think you need to look at setting TERMCMD and TERMCMDRUN to acceptable values. Your gnome-terminal looks broken.

0 项奖励
回复
4,737 次查看
shashankreddyvu
Contributor I

Thank you for your answer it is absolutely correct, i too tried same thing it worked for me.

I have one more dought

now am running systembuilder for p2041rdb board

now i am at "Add package patches and rebuild package" stage and i am trying to execute below command

bitbake -c clean <package-name>

here what is meant by package-name.

Thank you.

0 项奖励
回复
4,737 次查看
mattsm
Contributor III

The recipe name. So you can look for files in the following format: ${PN}_${VERSION}.bb, here PN = package name.

4,737 次查看
shashankreddyvu
Contributor I

HI,

Thank you for your answer, based on that i found package name as "rcw-p2041rdb", because of that i gone to next step but i got struct once again, I hope this may be my last dought

now i am in "Add package patches and rebuild package" stage, there they gave as below

/********************************************************************************/

Create amend.inc file and add following content in amend.inc file

                SRC_URI += "file://<name-of-patch1> \              

                file://<name-of-patch2> \

                ... \

                file://<name-of-patch n> \

                "

/********************************************************************************/

i didn't got what what to replace with "name of patch 1, name of patch 2 ......."

Thank you

0 项奖励
回复
4,737 次查看
mattsm
Contributor III

What error are you seeing with building rcw-p2041rdb? I don't think you should jump in to modify the recipe and/or patches.

-M

0 项奖励
回复
4,737 次查看
shashankreddyvu
Contributor I

Actually there was no error it was successful, The steps give are as below

/*****************************************************************************************************/

Add package patches and rebuild package

Add patches for a package (including u-boot and kernel) and rebuild this package as follows:

1. cd <system_builder_installation_path>

2. bitbake -c clean <package-name>

3. Create a new custom collection, for example, mycollection

mkdir -p mycollection/recipes/images

4. Create amend.inc file and add following content in amend.inc file

                SRC_URI += "file://<name-of-patch1> \               

                file://<name-of-patch2> \

                ... \

                file://<name-of-patch n> \

                "

5. Update the project configuration

./scripts/create-config.py --config-file=fsl-<bsp>/sample-create-config.ini --override-collection mycollection -j 4 -t 2

6. Rebuild this package with added patches.

bitbake <package-name>

/*****************************************************************************************************/

so in the 4th step is it not necessary no replace "name of the patch" with patch name. That was the thing i was asking.

Thank you.

0 项奖励
回复
4,737 次查看
mattsm
Contributor III

The 4th step is optional, only if you want to modify the recipe from another layer. In the example they use amend.inc to add some patches.

-M

4,737 次查看
shashankreddyvu
Contributor I
hi Matthew McClintock,

i want to use "fmc tool" on my host pc, but how to install it i didn't got it, i think the package is located at "/QorIQ-DPAA-SDK-20111026-systembuilder/fsl-packages-private/recipes/fmc/fmc-0.9.7-2".

please help me with how to install fmc tool on host pc,

Thank you.


0 项奖励
回复
4,737 次查看
mattsm
Contributor III

If build for the host, can you git clone the repo and find what you need standalone?

http://git.freescale.com/git/cgit.cgi/ppc/sdk/fmc.git/

0 项奖励
回复
4,737 次查看
shashankreddyvu
Contributor I

Thank you very much for clearing my doughts.

0 项奖励
回复