hello,my p4080ds linux sdk source code is download from https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk project
now i want to use usdpaa function with p4080,but i can't find p4080ds-usdpaa.dts in my source code,and i can't find example source code for usdpaa such as usdpaa-apps,how can i get the source code for reflector application,sra application and so on.
is it the linux sdk source code download from https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk don't support usdpaa? usdpaa is very import for me.
thanks yipingwang,i have install "QorIQ Linux SDK v2.0 SOURCE.iso" and "QorIQ SDK V2.0 PPCE500MC Yocto CACHE.iso" in the same path,i also resolved the two build problems:
[yocto] [pyro][bitbake][PATCH] bitbake: Replace deprecated git branch parameter "--set-upstream"
[pseudo-native] No real function for mknod
but when i build the linux system,the follow is errors:
branch 'origin/sdk-v2.0.x' does not exist
Task 1331 (/home/linux-develop/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-dpaa/usdpaa/usdpaa_git.bb, do_unpack) failed with exit code '1'
i guess the error is about " git -c core.fsyncobjectfiles=0 branch --set-upstream-to sdk-v2.0.x origin/sdk-v2.0.x"
how can i resolve the problem?
i have login www.nxp.com,
i don't find QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso and Cache ISO QorIQ-SDK-V2.0-PPCE500MC-CACHE-20160527-yocto.iso
Please download
"QorIQ Linux SDK v2.0 SOURCE.iso" and
"QorIQ SDK V2.0 PPCE500MC Yocto CACHE.iso"
thank you,but where can i download ISO QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso and Cache ISO QorIQ-SDK-V2.0-PPCE500MC-CACHE-20160527-yocto.iso? i don't find them at Linux® SDK for QorIQ® Processors | NXP
Please login www.nxp.com, then click "Download" from the above link.
my image boot log display "QorIQ SDK (FSL Reference Distro) 2.7+snapshot p4080ds ttyS0",is that meaning the version of yocto is 2.7?
Hello lixing gao,
Please download source ISO QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso and Cache ISO QorIQ-SDK-V2.0-PPCE500MC-CACHE-20160527-yocto.iso, then install both ISOs in the same path, you could build images without networking connection.
Thank,
Yiping
thanks for your reply,but QorIQ Linux SDK 2.0 release, which could be downloaded from Linux® SDK for QorIQ® Processors | NXP can't be compiled because www.freescale.com is shut down,which yocto verison support both
p4080ds and USDPAA
Hello lixing gao,
Yocto 3.0 release doesn't support USDPAA, you could use QorIQ Linux SDK 2.0 release, which could be downloaded from Linux® SDK for QorIQ® Processors | NXP .
Thanks,
Yiping