p4080 fabric details.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p4080 fabric details.

703 Views
softinvs
Contributor I

Hi All,

We're working on P4080 Virtulization(Porting legacy OS on third party core) and like to know few general things before ramp up:

- P4080 is said to provide 10Gb/s .

    - This bandwidth is related to any external hardware or the processor itself capable to support 10Gb/s?

    - Could anyone tell me about realistic bandwidth?

    - How much we can relate the CPU/core occupancy wrt bandwidth usage.?

Thanks in Advance...

Labels (1)
Tags (2)
0 Kudos
3 Replies

445 Views
jiantang
Contributor I

Hi SoftInv S:

  Do you have the throughput of 10Gb serdes ?

  I have the same question。

  If I configure the serdes to XAUI and extend a 10Gb Ethernet port. 

  then ,What is the throughput of 10Gb?for example: under Linux OS , the packet is 512 byte,

 

 

0 Kudos

445 Views
lunminliang
NXP Employee
NXP Employee

Hello jian tang,

You could refer to this thread for the information:

Does anyone test the 10-gigabit network's performance on P4080?

Some rough numbers given there.

Have a great day,
Lunmin

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos

445 Views
lunminliang
NXP Employee
NXP Employee

There is benchmark report about IPFWD describing this, including the soft and instrument configuration, also indicate relation to using core numbers, but this is NDA required, you need to contact sales for this issue.

0 Kudos