p2040 power sequencing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p2040 power sequencing

1,195 Views
dickginther
Contributor III

The sequencing for the P2040 states that:

1.  Bring up OVDD (3V3), LVDD (2V5), BVDD (3V3), CVDD (3V3), USB_VDD_3P3 (3V3)

2.  Bring up VDD_CA_CB_PL (1V0), SVDD (1V0), AVDD (1V0), USB_VDD_1P0 (1V0)

3.  Bring up GVDD (1.35V) and XVDD (1V5)

So step 1 has the 2.5V coming up the same time as the 3.3V. The sequence would be:  3.3V/2.5V -> 1V -> 1.35V/1.5V.  However the sequence for the P4080 evaluation board schematic shows the 2.5V coming up after the 3.3V (although the notes say "3.3V & 2.5V --->1.0V--->1.5V---->RST"), so does that suggest that the 2.5V delay after 3.3V is OK? 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,075 Views
lunminliang
NXP Employee
NXP Employee

I think items in the same section have no ordering requirement with respect to one another.

0 Kudos
Reply