p2020rdb SDK-1.9 u-boot booting problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p2020rdb SDK-1.9 u-boot booting problem

626 Views
matt_tsai
Contributor I

Hi,

I built the u-boot image from NXP SDK-1.9 and flash the image at NOR flash 0xeff40000. However, when the device starts, the serial console displays the following error:

U-Boot 2015.01+SDKv1.9+geb3d4fc (Dec 04 2015 - 07:52:10)

CPU0:  P2020E, Version: 2.0, (0x80ea0020)
Core:  e500, Version: 5.0, (0x80211050)
Clock Configuration:
       CPU0:1000 MHz, CPU1:1000 MHz,
       CCB:500  MHz,
       DDR:333.333 MHz (666.667 MT/s data rate) (Asynchronous), LBC:31.250 MHz
L1:    D-cache 32 KiB enabled
       I-cache 32 KiB enabled
Board: P2020RDB-PCA CPLD: V15.15 PCBA: V15.0
rom_loc: nor upper bank
SD/MMC : 4-bit Mode
eSPI : Enabled
I2C:   ready
SPI:   ready
DRAM:  DIMM 0: is not a DDR3 SPD.
SPD error on controller 0! Trying fallback to raw timing calculation
Detected UDIMM Fixed DDR on board
1 GiB (DDR3, 64-bit, CL=5, ECC off)

I have an old Freescale p2020rdb board (Rev. B) which uses DDR2 RAM.

Questions:

Can the u-boot be modified so that it can boot on this board? If yes, what needs to be changed?

Thank you for your help.

Labels (1)
Tags (1)
0 Kudos
1 Reply

399 Views
Pavel
NXP Employee
NXP Employee

Configuration of the u-boot is available in the following folder in u-boot source: /include/configs/.

Look at the configuration file for P2020RDB from SDK 1.9 in the attachment.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos