p2020 tcp throughput

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

p2020 tcp throughput

跳至解决方案
1,301 次查看
parkmanchan
Contributor I

Hi folks,

  What would be the expected TCP throughput on a P2020?

  I'm getting a Rx/Tx bandwidth of around 850Mbits/s when testing Rx/Tx separately, but when testing  Rx/Tx at the same time, the Rx throughput drops to less than 300Mbits/s, with Tx at around 800Mbits/s. What could be the problem here? Is this limited by the CPU?

Details of the test setup.

   PC1  -> P2020 eth0 -> PC2

   P2020 running Linux 2.6.35, TCP bandwidth testing with iperf 2.0.5

1. Rx bandwidth

    on the P2020

          iperf -s

    PC1

          iperf -c P2020_ip

2. Tx bandwidth

    on the P2020

          iperf -c PC2_ip

    PC2

          iperf -s

3. Runs 1 and 2 at the same time for testing Rx/Tx at the same time.

Thanks.

标签 (1)
0 项奖励
回复
1 解答
1,074 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Park man Chan,


Since you are using the old version Linux 2.6.35, the throughput should be a little lower than the expected result, with the latest SDK, the throughput is much better than your result. Not sure what is your testing frame size, because larger frame gets better throughput.


For the behavior Rx throughput dropping much than Tx, this should be normal, because for netperf(iperf) testing, the bottleneck is CPU.




Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,075 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Park man Chan,


Since you are using the old version Linux 2.6.35, the throughput should be a little lower than the expected result, with the latest SDK, the throughput is much better than your result. Not sure what is your testing frame size, because larger frame gets better throughput.


For the behavior Rx throughput dropping much than Tx, this should be normal, because for netperf(iperf) testing, the bottleneck is CPU.




Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复