we have 2 p1011 board that we run vxworks on.
1. Now I'm trying to configure the PCIE2 of board A p1011 for the RC.
I'm trying to configure the PCIE1 of board B p1011 for the EP(cfg_host_agt[0:2]=000,Device acts as an agent on all its PCI Express interfaces).
2. board A and board B are plugin the backboard.
3. when the backboard power on.
1)the boardA RC: LTSSM shows Detect quie; no pcie device found.
2)the boardB EP:
PCI_Bus @ 0x0038eea0 with bridge @ 0x003905a0
Device Instances:
Orphan Devices:
(null) unit 0 on PCI_Bus @ 0x0039dba0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039dca0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039dda0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039dea0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039dfa0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e0a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e1a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e2a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e3a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e4a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e5a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e6a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e7a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e8a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039e9a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039eaa0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039eba0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039eca0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039eda0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039eea0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039efa0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039f0a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039f1a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039f2a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039f3a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039f4a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039f5a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x0039f6a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x003a07a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x003a08a0 with busInfo 0x00000000
(null) unit 0 on PCI_Bus @ 0x003a09a0 with busInfo 0x00000000
4. when I put the boardA p1011 in the backboard, I put boardC(not p1011, a PCIE device) in the backboard, the backboard power on:
1) boardA p1011: LTSSM shows L0, vxBusShow can found the boardC.
so I think the configration of boardA p1011 RC is correct.
5 would you please give me some suggestion, how to config the EndPoint register of P1011?
Is this problem resolved?We have the same trouble,how did you resolved it?Thank!