Hi
Thanks for your reply and please find my response as mentioned below:
1. You're using customer board right? Can you share the schematic?
Ram" Yes we are using customer board. I may not share the complete
design, but if you need i can provide the information what you need.
sorry for this.
2. Did you succeed booting with correctly programmed NOR flash?
Ram: yes, our client has programmed flash in board which booted
successfully but as we don't have programmed parts, we have a blank NOR
flash on the board.
3. Did you try booting from alternate source? was it successfully booted?
Ram: I have tried to load code from Green Hills debugger, but as
processor HRESET is toggling continuously i was not succeeded.
4. Is I2C boot sequencer ON?
Ram: I2C boot sequencer is off.
5. Is this an isolated case or entire bulk faces this problem?
Ram: we have made two bulk of boards separately one at Client place and
another at our place. entire boards at our place is having this problem.
Regards,
Ramalinga Reddy