how to create a SMP bareboard project for P2020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to create a SMP bareboard project for P2020

848 次查看
yansongzhu
Contributor III

It seems that the codewarrior don't support SMP mode for P2020 ? So how to create a SMP bareboard project for P2020 by myself ?

标签 (1)
0 项奖励
回复
1 回复

687 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

I am not sure what do you mean as SMP mode of the P2020. But it is true the SMP option of Codewarrior Bareboard Project  is available for selection only while creating projects for some e500mc, e5500, and e6500 core targets. P2020 has the e500 core The e500mc is designed to be implemented in multicore integrated devices, and many of the features are defined to support multicore implementations.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复