how to create a SMP bareboard project for P2020

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to create a SMP bareboard project for P2020

852件の閲覧回数
yansongzhu
Contributor III

It seems that the codewarrior don't support SMP mode for P2020 ? So how to create a SMP bareboard project for P2020 by myself ?

ラベル(1)
0 件の賞賛
返信
1 返信

691件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

I am not sure what do you mean as SMP mode of the P2020. But it is true the SMP option of Codewarrior Bareboard Project  is available for selection only while creating projects for some e500mc, e5500, and e6500 core targets. P2020 has the e500 core The e500mc is designed to be implemented in multicore integrated devices, and many of the features are defined to support multicore implementations.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信