Please refer to SRIO example from MPC8569.
&rio {
compatible = "fsl,srio";
interrupts = <48 2 0 0>;
#address-cells = <2>;
#size-cells = <2>;
fsl,srio-rmu-handle = <&rmu>;
sleep = <&pmc 0x00080000>;
ranges;
port1 {
#address-cells = <2>;
#size-cells = <2>;
cell-index = <1>;
};
port2 {
#address-cells = <2>;
#size-cells = <2>;
cell-index = <2>;
};
};
For rmu definition, please refer to pq3-rmu-0.dtsi.
SPI controller dts node is added by default in pq3-espi-0.dtsi.
The following example is SPI devices definition in device tree.
spi@7000 {
flash@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "spansion,s25sl12801";
reg = <0>;
spi-max-frequency = <40000000>; /* input clock */
partition@u-boot {
/* 512KB for u-boot Bootloader Image */
reg = <0x0 0x00080000>;
label = "u-boot";
read-only;
};
partition@dtb {
/* 512KB for DTB Image*/
reg = <0x00080000 0x00080000>;
label = "dtb";
};
partition@kernel {
/* 4MB for Linux Kernel Image */
reg = <0x00100000 0x00400000>;
label = "kernel";
};
partition@fs {
/* 4MB for Compressed RFS Image */
reg = <0x00500000 0x00400000>;
label = "file system";
};
partition@jffs-fs {
/* 7MB for JFFS2 based RFS */
reg = <0x00900000 0x00700000>;
label = "file system jffs2";
};
};
slic@0 {
compatible = "zarlink,le88266";
reg = <1>;
spi-max-frequency = <8000000>;
};
slic@1 {
compatible = "zarlink,le88266";
reg = <2>;
spi-max-frequency = <8000000>;
};
};
Please make sure the device drivers are valid and enabled in Kernel.
Have a great day,
Yiping Wang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------