fsl-image-full on p1022ds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fsl-image-full on p1022ds

1,202 Views
doncook
Contributor II

When I build and run the fsl-image-full on the p1022ds, I was expecting the GUI to run by default. It doesn't, is there something else I need to add to the default build? I've expanded this to a broader group because it's really an SDK question.

0 Kudos
Reply
2 Replies

995 Views
lunminliang
NXP Employee
NXP Employee

I do not understand your question? The SDK does not provide feature for GUI.

0 Kudos
Reply

995 Views
doncook
Contributor II

The SDK provides a pre-configured image called fsl-image-full (among others), which I understand from the docs to be comparable to a desktop Linux distribution. When I build and load that image I don't get a display of that desktop GUI as I expected. My question is if this is normal for that build, or if something is missing in the startup to get that going.  I was hoping this would be a simple question for others that have built it before.

0 Kudos
Reply