external Watchdog timer program to reset the P2020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

external Watchdog timer program to reset the P2020

1,788 次查看
nareshpuli
Contributor III

hi,

i am trying to write a program for external watchdog timer , to reset the P2020 processor, help me.

how we write the program ?

标签 (1)
0 项奖励
回复
3 回复数

1,492 次查看
Pavel
NXP Employee
NXP Employee

Look at attached file. It is simple watchdog program example for the MPC8548. See the main.c file. The P2020 watchdog is the same as the MPC8548. Similar code can be used on the P2020 board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,492 次查看
nareshpuli
Contributor III

Hi Pavel Chubakov,

thanks for your reply, where is attached file, i can't find.

Regards

Naresh

Have a nice day...

0 项奖励
回复

1,492 次查看
nareshpuli
Contributor III

i got it...

0 项奖励
回复