consumption P2020 core 1 disabled and CHKSTP_IN1 forced to low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

consumption P2020 core 1 disabled and CHKSTP_IN1 forced to low

480 Views
philippeleray
Contributor II

Hi,

We use a P2020 on a board, and only core 0 is used, core 1 is not allowed to boot by configuration.

In case of the core 1 boot even of his boot configuration, we plan to pull-down the CHKSTP_IN1 pin.

Does the consumption will increase with this configuration ?

We don't see any current values with CHKSTP_IN1 maintaned to low level.

Labels (1)
Tags (3)
0 Kudos
1 Reply

320 Views
alexander_yakov
NXP Employee
NXP Employee

Assertion of CKSTP_IN causes all core clocks stopped, this actually disables the core, leaving only static leakages.

The total power consumption should decrease. The exact value may be roughly estimated by comparing power consumptions of P2020 and P2010 (single-core version of the same device). As I can see from two datasheets, this difference is not more than 10%


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos