hello experts
my new design use P1020 and i don't use USB function
in P1020 checklist if USB pins are not used they are pulled down by resistors
Data lines are 8 bit so i like to use common pull-donw resistor ( only USB STP is pulled up)
is it ok ?
thank you
Have a great day,
It is not ok. Do not use common pull-down resistor. There may be condition when connected pins are actively driven. For example you can see in the P1020 data sheet that if the I/O power supplies ramp prior to the VDD core supply, the I/Os associated with that I/O supply may drive a logic one or zero during power-up.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------