Hi all,
P1025 QE0 convolve a lot of pins as you see below. can we add exception on some of these pins?
for example can we set QE0 to 0 but CE_PB[10] treat as QE0 is 1?
my problem is on PB10 that alternate function is ENET5_TXD[1].
Regards
CE_ PA4 | LA16 | QE0 | LA16 | UPC1_ TxDATA[ 8] | ENET1_ RX_DV | TDMA_T XD[0] | SER1_ CTS | - | - | - | - |
CE_ PA5 | LA17 | QE0 | LA17 | UPC1_ TxDATA[ 9] | ENET1_ TX_EN | TDMA_ RXD[0] | SER1_ RTS | - | - | - | - |
CE_ PA6 | LA18 | QE0 | LA18 | UPC1_ TxDATA[ 10] | ENET1_ RXD[0] | TDMA_ TSYNC | SER1_ RXD[0] | - | - | - | BRGO9 |
CE_ PA7 | LA19 | QE0 | LA19 | UPC1_T xDATA[1 1] | ENET1_ TXD[0] | TDMA_R SYNC | SER1_ TXD[0] | - | - | - | BRGO10 |
CE_ PA8 | LA20 | QE0 | LA20 | UPC1_ TxDATA[ 12] | ENET1_ RX_ER | TDMA_R EQ | SER1_ CD | - | - | - | - |
CE_ PA9 | LA21 | QE0 | LA21 | UPC1_ TxDATA[ 13] | ENET1_ TXD[1] | - | - | - | - | - | - |
CE_ PA10 | LA22 | QE0 | LA22 | UPC1_ TxDATA[ 14] | ENET1_ RXD[1] | - | - | - | - | - | - |
CE_ PA11 | LDP0 | QE0 | LDP0 | UPC1_ TxDATA[ 15] | ENET1_ TXD[2] | TDMB_R XD[1] | SER3_ RXD[1] | - | - | - | - |
CE_ PA12 | LDP1 | QE0 | LDP1 | UPC1_ RxDAT A[8] | ENET1_ TXD[3] | TDMB_R XD[2] | SER3_ RXD[2] | - | - | - | - |
CE_ PA13 | LA28 | QE0 | LA28 | UPC1_ RxDAT A[9] | ENET1_ TX_ER | TDMB_R XD[3] | SER3_ RXD[3] | - | - | - | - |
CE_ PA14 | LGPL5 | QE0 | LGPL5 | UPC1_ RxDAT A[10] | ENET1_ RXD[2] | TDMB_T XD[1] | SER3_ TXD[1] | - | - | - | - |
CE_ PA16 | LCLK1 | QE0 | LCLK1 | UPC1_ RxDAT A[12] | ENET1_ COL | TDMB_T XD[3] | SER3_ TXD[3] | - | - | - | - |
CE_ PA17 | LA23 | QE0 | LA23 | UPC1_ RxDAT A[13] | ENET1_ CRS | - | - | - | - | - | - |
CE_ PA18 | LA24 | QE0 | LA24 | UPC1_ RxDAT A[14] | - | TDMD_T XD[0] | SER7_ CTS | 1588_clk_out | - | - | - |
CE_ PA19 | LA25 | QE0 | LA25 | UPC1_ RxDAT A[15] | - | TDMD_ RXD[0] | SER7_ RTS | 1588_pulse_ou t1 | - | - | - |
CE_ PA20 | LA26 | QE0 | LA26 | UPC1_ TxPRTY | - | TDMD_ TSYNC | SER7_ RXD[0] | 1588_trig_out | - | - | BRGO9 |
CE_ PA21 | LA27 | QE0 | LA27 | UPC1_ RxPRTY | - | TDMD_ RSYNC | SER7_ TXD[0] | 1588_tri g_in | - | - | BRGO11 |
CE_ PA22 | LCS4_B | QE0 | LCS4_B | UPC1_ RxSOC | - | TDMD_R EQ | SER7_ CD | 1588_pt p_clk | - | - | - |
CE_ PA23 | LCS5_B | QE0 | LCS5_B | UPC1_ TxSOC | - | - | - | - | - | CLK1, CLK12 | BRGO1 |
CE_ PA24 | LCS6_B | QE0 | LCS6_B | UPC1_ RxCLAV[ 0] | - | - | - | - | RISC_ GPIO[4] | CLK9 | BRGO2 |
CE_ PA25 | LA29 | QE0 | LA29 | UPC1_ TxCLAV[ 0] | - | - | - | - | RISC_ GPIO[5] | - | - |
CE_ PA26 | LA30 | QE0 | LA30 | UPC1_ TxEN[0] | - | - | - | - | - | - | - |
CE_ PA27 | LCS7_B | QE0 | LCS7_B | UPC1_ RxEN_B[ 0] | - | - | - | - | - | CLK6, CLK11 | BRGO1 |
CE_ PA30 | LA31 | QE0 | LA31 | UPC1_ TxADD R[2] | - | TDMB_ TSYNC | SER3_ RXD[0] | - | - | - | - |
CE_ PB10 | IRQ6 | QE0 | IRQ6 | - | ENET5_ TXD[1] | - | - | - | RISC_ GPIO[14 | CLK7, CLK16 | BRGO5 |
The only 10 QE port pins may be used to generate interrupts - PA4 PA8 PA18 PA22 PA28 PB0 PB4 PB8 PB14 PB18
Please look P1025 Reference Manual, Sections 3.5.3 and 3.5.4 for more information.
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------