can not enter x-window in SDK 1.5 Ubuntu 13.04(P1020)

cancel
Showing results for 
Search instead for 
Did you mean: 

can not enter x-window in SDK 1.5 Ubuntu 13.04(P1020)

177 Views
limingcui
Contributor I

Hello.

I plan to build an image for P1020.

I am using SDK  1.5, Ubuntu 13.04.

I have setup the host enviroment.

As succeeding to complete command of host-prepare.sh, and if rebooting computer, I cannot enter x-window forever,

I am sure passwd is right, and if not rebooting computer, I can compile kernel, module, everything is ok.

I reinstall Ubuntu 13.04 and repeat above-mentioned procedure, nothing change.

It looks like that SDK1.5 package updating damage some system file of ubuntu 13.04 

Labels (1)
Tags (1)
0 Kudos
0 Replies