ath10k driver on p1020-wlan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ath10k driver on p1020-wlan

1,122 Views
nimeshkanoth
Contributor I

HI all,

we are integrating atheros AR9882 WIFI Chipset via MiniPCI-Express 1.1 host interface on P1020-WLAN Board, for this we backported ath10k driver for kernel 2.6.32. after inserting the drivers we are getting following PCI errors.

root@FSL:/# insmod compat.ko
Loading modules backported from Linux version v3.14-0-g455c6fd
Backport generated by backports.git v3.14-1-0-g369d49a
root@FSL:/# insmod compat_firmware_class.ko
root@FSL:/# insmod cfg80211.ko
cfg80211: Calling CRDA to update world regulatory domain
root@FSL:/# insmod mac80211.ko
root@FSL:/# insmod ath.ko
root@FSL:/# insmod ath10k_core.ko
root@FSL:/# insmod ath10k_pci.ko
ath10k_pci 0001:03:00.0: BAR 0: can't allocate mem resource [0x80000000-0x801fffff]
ath10k: eef7fcf8
ath10k_pci: probe of 0001:03:00.0 failed with error -16

please guide us to solve the issue.

Thanks,

NImesh

Labels (1)
0 Kudos
1 Reply

429 Views
bpe
NXP Employee
NXP Employee

You are using a kernel that is really ages old. I don't think we can share any experience with it and modern radio cards. Based on the error your kernel throws, there is insufficient space in the PCI window. Normally, u-Boot sets

much larger PCI windows than the space you device requests. The suggestions are:

1. Check what windows your u-Boot allocates to PCI

2. Check your device tree "ranges" property to make sure they

   are properly reflect the size of the window allocated by u-Boot.

   Details can be found here:

   http://elinux.org/Device_Tree_Usage#Ranges_.28Address_Translation.29

   http://elinux.org/Device_Tree_Usage#PCI_Host_Bridge

3. If everything looks correct but still no luck, debug the kernel.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos