With SETA=1 is the external LGTA exempt from the bus monitor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

With SETA=1 is the external LGTA exempt from the bus monitor?

Jump to solution
523 Views
sapril
Contributor I

Hi -

I am using a P1020 with the local bus configured with SETA = 1 for CS4. 

The manual says for sure that if SETA = 1, ONLY LGTA can terminate a transaction; internal TA is completely ignored.

So, does that mean that External TA is exempt from bus monitor? 

Labels (1)
0 Kudos
1 Solution
435 Views
LPP
NXP Employee
NXP Employee

When SETA =1 then an access is terminated either by LGTA assertion or by

the bus monitor whatever happens earlier.

View solution in original post

0 Kudos
2 Replies
436 Views
LPP
NXP Employee
NXP Employee

When SETA =1 then an access is terminated either by LGTA assertion or by

the bus monitor whatever happens earlier.

0 Kudos
435 Views
alexander_yakov
NXP Employee
NXP Employee

In case if internal TA generation is disabled by SETA, local bus GPCM controller will wait for external TA (LGTA) assertion.

If there is no external TA assertion within reasonable time, bus monitor will terminate this transaction and generate TEA ("transfer error acknowledge").