Why does system hang when I set CE_PA22 as high leve? Does LBC multiplexed GPIO pins can not be used as GPIO when LBC is enabled?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does system hang when I set CE_PA22 as high leve? Does LBC multiplexed GPIO pins can not be used as GPIO when LBC is enabled?

434 Views
carlpeng
Contributor II

Hello,

Why does system hang when I set CE_PA22 as high leve or low level?

In my platform, we use NOR flash with the LBC cs0, meanwhile, we want to use CE_PA22 as an output GPIO, 

but when I set CE_PA22 as high level, system will hang, when set as low level, also will hang.

Could please help to give some suggestions?

Thank you,

Carl

Labels (1)
0 Kudos
1 Reply

317 Views
alexander_yakov
NXP Employee
NXP Employee

Please specify what you exactly doing in terms of hardware - i.e. which address locations you are writing, and with this values exactly.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos