Which COP J-TAG tool is most preferred to P2040 and Why? (Code Warrior TAP or Code Warrior USB TAP)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which COP J-TAG tool is most preferred to P2040 and Why? (Code Warrior TAP or Code Warrior USB TAP)

544 Views
nsuvarnak
Contributor I

Basically there are two J-tag tools available at NXP,

1)CWH-CTP-COP-YE

2)CWH-UTP-CF-HE

Labels (1)
Tags (1)
0 Kudos
1 Reply

430 Views
alexander_yakov
NXP Employee
NXP Employee

CWH-CTP-COP-YE - is not a complete debug probe, this is only a tip, you need also to order CodeWarrior TAP "base unit":

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

Second partnumber "CWH-UTP-CF-HE" is old "CodeWarrior USB TAP" debug probe, which is no longer manufactured, and also this partnumber is not suitable for P2040 because suffix "CF" means "ColdFire" processors, for P2040 you have to use "COP" version, partnumber is CWH-UTP-PPCC-HE


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------