Where is the hv.dts file in Freescale SDK 1.6 for P4080DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the hv.dts file in Freescale SDK 1.6 for P4080DS

Jump to solution
2,186 Views
peterzheng
Contributor II

Hi,

I was trying to create 8 partitions on P4080DS using hypervisor.  I was following the documentation provided by Yiping.

https://community.freescale.com/docs/DOC-102249

However, I have trouble locate the hv.dts file. Could you help me with this issue? where is this file in the SDK after uncompress the ISO?

Thanks,

Peter Zheng

Labels (1)
0 Kudos
Reply
1 Solution
1,817 Views
lunminliang
NXP Employee
NXP Employee

Hi,

Please check in attached hv-cfg-fsl-sdk-v1.6.tar.gz for SDK, under the path /p4080ds/R_PPSXX_0xe/hv-2p-Lnx-Lnx/hv.dts.

Also you can download from below for SDK1.6:

sdk/hv-cfg.git - Freescale PowerPC Hypervisor Config Tree

root/p4080ds/R_PPSXX_0xe/hv-2p-lnx-lnx/hv.dts

Is this what you want?


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,818 Views
lunminliang
NXP Employee
NXP Employee

Hi,

Please check in attached hv-cfg-fsl-sdk-v1.6.tar.gz for SDK, under the path /p4080ds/R_PPSXX_0xe/hv-2p-Lnx-Lnx/hv.dts.

Also you can download from below for SDK1.6:

sdk/hv-cfg.git - Freescale PowerPC Hypervisor Config Tree

root/p4080ds/R_PPSXX_0xe/hv-2p-lnx-lnx/hv.dts

Is this what you want?


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,817 Views
peterzheng
Contributor II

Hi Lunmin,

Thank you for your help. Could you help me take a look at another problem?

how to create 8 partitions using hypervisor in P4080DS

Thanks & Regards,

Peter Zheng

0 Kudos
Reply
1,817 Views
lunminliang
NXP Employee
NXP Employee

Hi,

Sure, I'll have a look soon later.

Regards

Lunmin

0 Kudos
Reply
1,817 Views
peterzheng
Contributor II

Hi Lunmin,

I was pointing you to the wrong question. Sorry about that. Can you take a look at this particular question?

How to partition the L3 Cacahe of P4080 using CodeWarrior?

Thank you very much for your time and help!

Regards,

Peter

0 Kudos
Reply