Hi,
I was trying to follow the document to set up the environment in p4080ds.
http://cache.freescale.com/files/soft_dev_tools/doc/support_info/QorIQ-SDK-1.6-IC-RevB.pdf
When I reach the 4.2.1.3 Configuring U-Boot network Parameters, it requires me to set the MAC addresses. May I ask where can I find the correct MAC addresses?
Thanks & Regards,
Peter
Hello Peter Zheng,
In MAC address, the first 24 bits are OUI(Organizationally Unique Identifier), which is from IEEE for each factory. The rest 24 bits are set by factory.
Here 00-04-9F is for Freescale and 00-E0-0C is for MOTO. For test purpose, I think you can set MAC yourself, just make it differs from other MAC in your locally administered address space.
00-E0-0C (hex) MOTOROLA
00E00C (base 16) MOTOROLA
5401 N. BEACH ST. S243
FT. WORTH TX 76137
UNITED STATES
00-04-9F (hex) Freescale Semiconductor
00049F (base 16) Freescale Semiconductor
7700 West Parmer Lane
MD PL59
Austin TX 78729
UNITED STATES
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------