Where can I find the Linux application examples for p4080ds

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find the Linux application examples for p4080ds

764件の閲覧回数
gaolixing
Contributor I

hello,i am new to p4080ds,now i can compile a "hello world" program for p4080ds,and it run successfully on p4080ds,but p4080 is a complex soc,Where can I find the Linux application examples for p4080ds,for example,linux application example for DPAA,PCIE,and so on

ラベル(1)
0 件の賞賛
2 返答(返信)

704件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Sections 7.4, 7.11 in SDK 1.9 documentation:

https://freescaleesd.flexnetoperations.com/337170/647/10318647/QORIQ-SDK-1-9_RN.pdf?ftpRequestID=776...

 

These documentation contains information about using DPAA, PCI and other interfaces for SDK 1.9 Linux BSP.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

705件の閲覧回数
gaolixing
Contributor I

and where can i find the manual for the specific linux api for p4080 soc in sdk2.0 version

0 件の賞賛