What kind of output drive is HRESET_REQ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What kind of output drive is HRESET_REQ?

981 Views
adamgarrison
Contributor III

A question came up about the HRESET_REQ pin on the P1022. We’re wondering what kind of output driver this is – is it an open drain? We’ve currently got it connected in parallel with our reset button, which has been working fine, but we’re worried that if it is driving high then we will short it to ground when we push the button. So far there’s been no damage, but I just want to make sure I don’t need to make a change on our board.  I’m moving ahead with it designed how I have it, it seems to work fine, but I would love to double check my assumption.

Thanks,

Adam

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

825 Views
ufedor
NXP Employee
NXP Employee

Described connection is incorrect.

1) The HRESET_REQ_B is an actively driven output

2) The HRESET_REQ_B can't be used to drive HRESET_B directly because HRESET_REQ_B  is deasserted immediately after HRESET_B assertion is detected. Resulting HRESET_B pulse violates requirement (25 us minimum) of the P1022 QorIQ Integrated Processor Hardware Specifications, Table 5. RESET initialization timing specifications.

It is recommended to handle the HRESET_REQ_B by a CPLD.


Have a great day,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply