What is the input current on P1013 power supply pins : AVDD_PLAT,AVDD_COREn, AVDD_DDR, SDAVDD, and SDAVDD2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the input current on P1013 power supply pins : AVDD_PLAT,AVDD_COREn, AVDD_DDR, SDAVDD, and SDAVDD2

362 Views
williamweishaup
Contributor II

I need to know what the input current is for each of the PLL input pins (AVDD_PATT, AVDD_COREn, AVDD_DDR, SDAVDD, and SDAVDD2) on the P1013 so I can select the proper wattage of the series resistor and meet my derating requirement for these resistors

Labels (1)
0 Kudos
1 Reply

281 Views
ufedor
NXP Employee
NXP Employee

Consumed currents are:

each AVDD <= 5 mA

each SDAVDD <= 20 mA

0 Kudos