Unable to locate P1020RDB I2C pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to locate P1020RDB I2C pins

865 Views
bilalwasim
Contributor II

I want to use the functionality of I2C (as well as SPI) on the P1020RDB board. However, seeing the schematics, I'm unable to locate the exact pins I should be using for I2C. In the schematics, it says that the U41D IC is responsible for dealing with I2C and SPI. However, on my board there is only U41, and not U41A, U41B etc. Seems to me that I have the wrong assembly diagrams. However, I'm unable to find any other reference manuals as well.

I'm using the P1020RDB with the Red casing, and not this one https://encrypted-tbn0.gstatic.com/images?q=tbn:ANd9GcRZqqsb1I5dUkv3cWx462t2nSWpXLuL-JBVwmpDfW4CtpoQ...

Any help would be appreciated.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

658 Views
ufedor
NXP Employee
NXP Employee

Please provide information printed on the case sticker and on-board sticker(s) and markings.

0 Kudos
Reply

658 Views
bilalwasim
Contributor II

Its P1020RDB RevD. There's a sticker on the back "SCH-26158 REV-D". I've got nothing else :smileysad:

0 Kudos
Reply

658 Views
ufedor
NXP Employee
NXP Employee

Please open a technical case to obtain the RDB schematics:

https://community.freescale.com/thread/381898

0 Kudos
Reply