Thermal diode interface to monitor temperature in P1022 processor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Thermal diode interface to monitor temperature in P1022 processor?

Jump to solution
722 Views
prasantahalder
Contributor II

We are using P1022 in one of our design. According to its datasheet, Pin-B26 and A27 is to not connected whereas it is used in its reference design as thermal diode's anode and cathode. Can it be used as thermal diode interface to monitor temperature using MAX6695 type of devices?

Labels (1)
1 Solution
454 Views
Pavel
NXP Employee
NXP Employee

The main problem for similar connection is parameters of this thermal diode.

The P1022 Datasheet does not have information about thermal diode parameters. You should calibrate this thermal diode for thermal measurement.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
454 Views
prasantahalder
Contributor II

I mean to ask whether thermal diode anode and cathode(Pin-B26 and A27) of P1022 can be connect to MAX6695's remote diode pins to measure the temperature as done in P1022DS schematic using ADT7461 IC.

0 Kudos
455 Views
Pavel
NXP Employee
NXP Employee

The main problem for similar connection is parameters of this thermal diode.

The P1022 Datasheet does not have information about thermal diode parameters. You should calibrate this thermal diode for thermal measurement.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

454 Views
Pavel
NXP Employee
NXP Employee

The P1022 Datasheet shows that these pins are no connects.

These pins cannot be used for the MAX6695 connection.

Use I2C interface of the P1022 for the MAX6695 connection.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos