The mechanics of switching between user/supervisor/hypervisor mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The mechanics of switching between user/supervisor/hypervisor mode

ソリューションへジャンプ
1,507件の閲覧回数
mikelackey
Contributor I

I am looking for a P4080/e500mc document that describes the mechanics of writing code to switch between user/supervisor/hypervisor mode.  I'm new to this, and not sure how it works.  I've looked in the e500mc ref manual, the P4080 programmer's manual, google, and this community.  I'm probably not asking the right question.

My SWAG is that privilege is controlled by the MMU configuration.  Example, say three small-ish blocks of virtual memory, one configured with user only privs, one with supervisor privs, and one with hypervisor privs.  At startup the code (by default running in hypervisor space) configures the MMU to provide three blocks of memory, such that each block has differing privs.  When initialization is complete, jumping to the address space of another block automagically updates the MSR.  Stated differently, the MSR is changed to what is configured for that block.  So there really is no code to switch back and forth, just transferring control from one block to another causes the MSR to be updated with the privs assigned to that block.

Is there a doc that describes the mechanics of this?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,306件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Attempting to access hypervisor or supervisor resources or instructions causes privilege exceptions, which the operating system can handle appropriately. When core jumps to the privelege exception handler the MSR is changed as it required for the privilege level. There is System Call instruction to generate a system call or a hypervisor-level system call (hypercall) interrupt. It permits a program to call on the system to perform a service or an operating system to call on the hypervisor to perform a service. See section 3.4.5.6 System Linkage Instruction in the e500mc document. You also can look section 1.2.3 Privilege Model in the EREF: A Programmer’s Reference Manual for Freescale Power Architecture Processors https://www.nxp.com/files-static/32bit/doc/ref_manual/EREF_RM.pdf

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,307件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Attempting to access hypervisor or supervisor resources or instructions causes privilege exceptions, which the operating system can handle appropriately. When core jumps to the privelege exception handler the MSR is changed as it required for the privilege level. There is System Call instruction to generate a system call or a hypervisor-level system call (hypercall) interrupt. It permits a program to call on the system to perform a service or an operating system to call on the hypervisor to perform a service. See section 3.4.5.6 System Linkage Instruction in the e500mc document. You also can look section 1.2.3 Privilege Model in the EREF: A Programmer’s Reference Manual for Freescale Power Architecture Processors https://www.nxp.com/files-static/32bit/doc/ref_manual/EREF_RM.pdf

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,306件の閲覧回数
mikelackey
Contributor I

Thank you.

0 件の賞賛
返信