The DDR SDRAM timing configuration 4 register (TIMING_CFG_4)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The DDR SDRAM timing configuration 4 register (TIMING_CFG_4)

3,140 Views
yansongzhu
Contributor III

I can't understand the function of RWT which is a part of TIMING_CFG_4.

"Read-to-write turnaround for same chip select
Specifies how many cycles are added between a read to write turnaround for transactions to the same
chip select. If a value of 0000 is chosen, then the DDR controller uses the value used for transactions to
different chip selects, as defined in TIMING_CFG_0[RWT]. This field can be used to improve performance
when operating in burst-chop mode by forcing transactions to the same chip select to use extra cycles,
while transaction to different chip selects can utilize the tri-state time on the DRAM interface. Regardless
of the value that is set in this field, the value defined by TIMING_CFG_0[RWT] also is met before issuing a
write command."

How this field used to improve performance when operating in burst-chop mode?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

813 Views
Bulat
NXP Employee
NXP Employee

Actually that field can not improve performance when operating in burst-chop mode. We have not revised that statement since first publication. We recommend to leave TIMING_CFG_4[RWT] with zero value, meaning the read-to-write turnaround time is the same for both cases: transactions to the same chip select and different chip selects.

Regards,

Bulat