SRA application on p2041rdb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SRA application on p2041rdb

跳至解决方案
1,449 次查看
norabjorklund
Contributor II

Hi,

I am trying to run the sra application on p2041rdb, but cannot get it working well. I compared it by running the same application and commands on t4240qds. And I was wondering what the problem could be.

When I start up the application I receive the following message:

sra: dma_usmem_init(): dma_mem_create(): Invalid argument

sra: dma_pool_init(): DMA pool: Invalid argument

I ran the first example in the SRA guide [1] And at the second step I received a segfault:

sra> sra -attr port1 win_attr 1 nwrite nread

sra> sra -op port1 1 0 0 s 0x100000

sra[1665]: unhandled signal 11 at 00000000 nip 0fec49d0 lr 100022f4 code 30001

Segmentation fault

(Running the same steps on t4240qds works well)

I am running fsl-image-core with the extra kernel configurations mentioned in th UG.

Best regards,

Nora

-----------

[1] Submit Form

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,191 次查看
norabjorklund
Contributor II

The usdpaa_mem boot argument was the error, I had in accordance with the SRA UG given usdpaa_mem=512M however for p2041 and p3041 this is too large. The sra application worked properly with usdpaa_mem=64M.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,192 次查看
norabjorklund
Contributor II

The usdpaa_mem boot argument was the error, I had in accordance with the SRA UG given usdpaa_mem=512M however for p2041 and p3041 this is too large. The sra application worked properly with usdpaa_mem=64M.

0 项奖励
回复