Hi,
we are using p1022 processor based custom board.we have used SDK1.9 with full package and able to boot linux on it from flash.As the file-system size is more than 25MB(compressed) ,it is taking so much time to boot.
so we have decided to run "fsl-image-minimal" package to get reduced filesystem.
But while running the command "bitbake fsl-image-minimal" in the sdk1.9,we are receiving the "oe_runconf failed" error.
so,please kindly help me in this issue.
Please find the attached log for more details...
thank you...
Regards,
Santosh kumar.
Original Attachment has been moved to: log.do_configure.20226.zip
Hello Santosh Kumar Aki,
I use SDK v1.9 for P1020rdb. I use this commands for your reference.
Ubuntu 14.04.4 LTS 32-bit
>>sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos
>>ls -l /bin/sh
>>sudo dpkg-reconfigure dash
Install the SDK cache for e500v2 and SDK
>> sudo mount -o loop QorIQ\ SDK\ V1.9\ PPCE500V2\ CACHE.iso /mnt/cdrom/
>> sudo /mnt/cdrom/install
>> sudo mount -o loop QorIQ\ SDK\ V1.9\ SOURCE.iso /mnt/cdrom
>> sudo /mnt/cdrom/install
>> ./sources/meta-freescale/scripts/host-prepare.sh
using the command "/usr/sbin/visudo"
>>. ./fsl-setup-env -m p1020rdb
>> bitbake fsl-image-full
Hello Santosh Kumar Aki,
The error is caused by lacking "/bin/mktemp" on your host machine, after install the ISO, please execute the script "sources/meta-freescale/scripts/host-prepare.sh" to deploy the necessary environment to use Yocto on the host.
In addition, please remember to install the Cache ISO to avoid building everything from the scratch.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------