Using the Yocto SDK v1.4, I have built an image for the p4080ds and attempted to boot it on my P4080PCIe demo board (this worked out of the box for v1.2). With v1.4, I get a BMAN error from dpaa_eth.c line 488 (bman_new_pool() failed) followed by a kernel invalid page request (and the termination of my boot process). I have tried disabling the BMAN in my kernel menuconfig, but then I no longer have Ethernet interfaces. Is there a mechanism to boot SDK v1.4 on a P4080 with Ethernet?
0. Please make sure all your images are part of the same SDK release
1. Please post a complete boot log (from board reset to the kernel stack dump)
2. The DPAA/Ethernet will not work without BMan
3. Erase the environment sector from bank 0 and the defaults should get you a usable console
More Information:
I am probably running the U-Boot version that was on the board when it shipped. I tftp a new image into ram and boot from memory. I have a working 1.2 image in flash that I can boot from. I do not want to flash over my working image and I have not been able to successfully boot into the alternate bank (serial speed appears incorrectly set for the alternate bank). Disabling DPAA Ethernet also works, but then I have no interfaces.
Error Information:
Freescale FM module (Jun 5 2014:10:08:39), FMD API version 21.1.0
Freescale FM Ports module (Jun 5 2014:10:08:40)
dpaa_debugfs: FSL DPAA Ethernet debugfs entries ()
fsl_mac: mac.c:417:mac_load() fsl_mac: FSL FMan MAC API based driver ()
fsl_mac ffe4e2000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:02:01:fd
cpu0: Applying 10G TX ECC workaround (10GMAC-A004) ...
cpu0: FAILED!
cpu0: ! MINOR FM-MAC Error [CPU00, drivers/net/ethernet/freescale/fman/Peripherals/FM/MAC/tgec.c:829 TgecInit]: Operation Timed Out;
cpu0: TgecTxEccWorkaround FAILEDcpu0:
fsl_mac ffe4f0000.ethernet: FMan XGEC version: 0x0001032c
fsl_mac ffe4f0000.ethernet: FMan MAC address: 00:04:9f:02:04:fd
cpu0: Applying 10G TX ECC workaround (10GMAC-A004) ...
cpu0: FAILED!
cpu0: ! MINOR FM-MAC Error [CPU00, drivers/net/ethernet/freescale/fman/Peripherals/FM/MAC/tgec.c:829 TgecInit]: Operation Timed Out;
cpu0: TgecTxEccWorkaround FAILEDcpu0:
fsl_mac ffe5f0000.ethernet: FMan XGEC version: 0x0001032c
fsl_mac ffe5f0000.ethernet: FMan MAC address: 00:04:9f:02:09:fd
fsl_dpa: dpaa_eth.c:4320:dpa_load() fsl_dpa: FSL DPAA Ethernet driver ()
fsl_dpa ethernet.17: Using private BM buffer pools
fsl_dpa: dpaa_eth.c:488:dpa_bp_alloc() bman_new_pool() failed
Unable to handle kernel paging request for data at address 0x0000002c
Faulting instruction address: 0xc05f2c54
Oops: Kernel access of bad area, sig: 11 [#1]
SMP NR_CPUS=8 P4080 DS
Modules linked in:
NIP: c05f2c54 LR: c05f3170 CTR: c02966b0
REGS: e9095b80 TRAP: 0300 Not tainted (3.8.13-rt9-QorIQ-SDK-V1.4)
MSR: 00029002 <CE,EE,ME> CR: 22a88e28 XER: 20000000
DEAR: 0000002c, ESR: 00000000
TASK = e907c9b0[1] 'swapper/0' THREAD: e9094000 CPU: 0
GPR00: c05f3170 e9095c30 e907c9b0 e9584c00 e967bb90 00000000 c0296f10 00000000
GPR08: c07dc4bc c0885fc4 0000002c 000000f8 000000f8 00000000 c0002650 00000002
GPR16: 00000000 ffffffff ffffffed e95e9528 e9095d58 c03e2000 00000001 e967bb90
GPR24: c0885fc4 c0626dc8 00000000 c07380e4 c0738b80 c0885fc4 e9584c00 00000000
NIP [c05f2c54] dpa_bp_free+0x48/0x158
LR [c05f3170] dpa_bp_create+0x2d0/0x31c
Call Trace:
[e9095c30] [c03e2000] dpa_bp_depletion+0x0/0x60 (unreliable)
[e9095ca0] [c05f3170] dpa_bp_create+0x2d0/0x31c
[e9095d30] [c03e2550] dpaa_eth_probe+0x4f0/0x1060
[e9095df0] [c02a8d28] driver_probe_device+0x88/0x260
[e9095e10] [c02a8fbc] __driver_attach+0xbc/0xc0
[e9095e30] [c02a6cfc] bus_for_each_dev+0x5c/0xb0
[e9095e60] [c02a8288] bus_add_driver+0x1a8/0x2a0
[e9095e80] [c02a9768] driver_register+0x88/0x1c0
[e9095eb0] [c07b33f8] dpa_load+0x5c/0xa4
[e9095ed0] [c0002088] do_one_initcall+0x148/0x1b0
[e9095f00] [c07968e4] kernel_init_freeable+0x12c/0x1e4
[e9095f30] [c0002664] kernel_init+0x14/0x110
[e9095f40] [c000eb70] ret_from_kernel_thread+0x64/0x6c
Instruction dump:
3be00000 3ba95fc4 48000118 1d3f0030 815e0004 7d2a4a14 89290004 5529103a
7d3d4a14 83490008 395a002c 7c2004ac <7d205028> 3129ffff 7d20512d 40a2fff4
---[ end trace 7a5a2d940788f3d5 ]---
Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
Rebooting in 180 seconds..