SATA init issues on P5020 with kernel 3.17-rc3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SATA init issues on P5020 with kernel 3.17-rc3

2,450 Views
RabbitHoleComp
Contributor II

        Has anyone here successfully built and booted a recent kernel from mainline? I have one built, however upon boot, sata init fails. Are there any known SATA-related erratum that I should be patching for?

Labels (1)
0 Kudos
Reply
7 Replies

2,029 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Alex Perez,

Would you please provide your u-boot and Kernel boot log?

What is the revision of P5020 used?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,029 Views
RabbitHoleComp
Contributor II

yipingwang

Sure, I can provide a kernel boot log. The P5020 I am using is production/shipping silicon. If you can tell me how to verify (via /proc or similar mechanism) which version it is, I'll be happy to double-check.

0 Kudos
Reply

2,029 Views
scottwood
NXP Employee
NXP Employee

U-Boot prints the SoC version in the boot messages.

0 Kudos
Reply

2,029 Views
scottwood
NXP Employee
NXP Employee

In Custom kernel for T4240qds - boot issues you said that the patches I linked to resolved your SATA problems -- are there any remaining issues?

0 Kudos
Reply

2,029 Views
RabbitHoleComp
Contributor II

scottwood, I see that the necessary SATA patches have made it in to mainline as of 3.18, however as previously stated, I have a machine which (using both 3.17-rc3 AND 3.18.1, does not enumerate any PCI devices on the tree. Are there any known patchsets to resolve this?

0 Kudos
Reply

2,029 Views
scottwood
NXP Employee
NXP Employee

Please post a new topic for the PCI issue, with a boot log and other relevant information.

0 Kudos
Reply

2,029 Views
RabbitHoleComp
Contributor II

Yes, those patches definitely resolve my SATA issues, however no PCI devices are enumerating on the bus (lspci returns nothing)

As for silicon revision, I am at 2.0:

U-Boot 2014.04-00110-g021fb01-dirty (Aug 20 2014 - 12:43:46)

CPU0:  P5020, Version: 2.0, (0x82200020)

Core:  e5500, Version: 1.2, (0x80240012)

0 Kudos
Reply