Requirement of Serdes Reference Clock in P5040 Processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Requirement of Serdes Reference Clock in P5040 Processor

ソリューションへジャンプ
1,180件の閲覧回数
prasantahalder
Contributor II

Hi,

We need to use two x1 PCIe and four SGMII of P5040. For that we are planning to use SRDS_PRTCL=04h and we connected two serdes lanes(SD4-SD5) for PCIeand four serdes lanes(SD6-SD9) as SGMII. We are not using Serdes Bank-2, Bank-3 and Bank-4.

For this configuration we are feeding 100MHz clock only in SD_REF_CLK1_N/P while other reference clocks are grounded. Is this scheme is OK or should we provide clock in other reference clock inputs?

Regards,

Prasanta

ラベル(1)
0 件の賞賛
返信
1 解決策
1,032件の閲覧回数
ufedor
NXP Employee
NXP Employee

> For this configuration we are feeding 100MHz clock only in SD_REF_CLK1_N/P

> while other reference clocks are grounded.

This configuration is viable.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,033件の閲覧回数
ufedor
NXP Employee
NXP Employee

> For this configuration we are feeding 100MHz clock only in SD_REF_CLK1_N/P

> while other reference clocks are grounded.

This configuration is viable.

0 件の賞賛
返信