Request_irq Flag mismatch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request_irq Flag mismatch

5,881 Views
lgerhard
Contributor I

I'm facing a problem with request_irq, when I try to hook my interrupt handler with the interrupt line, I receive the following message:

root@device:~# insmod kernelModule.ko
genirq: Flags mismatch irq 18. 00000000 (xyz) vs. 00000000 (xyz)
Request_irq return: -16 (This is my print of the return value of request_irq function)

The flags are totally equal, and I don't know what is the problem.

The irq number looks correct, as shown below:

root@device:~# cat /proc/interrupts
           CPU0       CPU1       CPU2       CPU3       CPU4       CPU5       CPU6       CPU7
  18:         0          0          0          0          0          0          0          0   OpenPIC     8 Level     xyz
 
 
And my code is listed below:
 
#define XYZ_IRQ         (18)

int reqRet;

static irqreturn_t xyz_interrupt(int irq, void *dev)
{
 printk(KERN_INFO "Interrupt "XYZ Handled!!!);
    return IRQ_HANDLED;
}
 
static int __init hello_init(void)
{
 reqRet = request_irq(XYZ_IRQ, xyz_interrupt, 0, "xyz", (void*)&reqRet);          
// reqRet = request_irq(XYZ_IRQ, xyz_interrupt, 0, "xyz", (void*)NULL); /* If I use this call, I don't receive the mismatch message, but the return code still -16 */
 printk(KERN_INFO "xyz_irq: Request_irq return: %d\n", reqRet);
 
    if(reqRet)
    {
  printk(KERN_ERR "xyz_irq: cannot register IRQ %d\n", XYZ_IRQ);
        return -EIO;
    }
 
 return 0;
}

My Device tree config for this external device:

xyz@5,0 {

   compatible = "generic-uio";

   reg = <0x5 0x0 0x1000>;

   interrupt = <0x8 0x1 0x0 0x0>

};

My device is based on p4080ds.
 
Could someone help me?

Thanks in advance

Labels (1)
0 Kudos
Reply
1 Reply

2,267 Views
Pavel
NXP Employee
NXP Employee

Look at the following page:

http://www-numi.fnal.gov/offline_software/srt_public_context/WebDocs/Errors/unix_system_errors.html

 

Error -16 shows about EBUSY for this interrupt.

 

See the following pages:

http://www.makelinux.net/books/lkd2/ch06lev1sec3

http://www.makelinux.net/ldd3/chp-10-sect-2

https://www.opennet.ru/man.shtml?topic=request_irq&category=9&russian=2

https://lists.gt.net/linux/kernel/883644


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply