Regarding etsec controller of P1022

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding etsec controller of P1022

791 Views
rinkutakkar
Contributor I

Hi,

We are having issues with the link stability of Ethernet switch and PHY devices connected to the Serdes of processor P1022. Following is the used serdes configuration:- 

cfg_serdes_ports : 10101 

We are using both ethernet controllers in SGMII mode. We have two different assembly options for the card with only a slight difference in the processor schematic.Following are the observation for both options:- 

Card 1: Both data path and control path(MIIM interface) for ETSEC 2 are working properly. 
Card 2 : MIIM interface is not stable. Only like 10% of the times it reads correct values, otherwise random results are observed on the MDIO line. Data path is not working at all when link gets up at 1000 MBps, with 100 MBps speed link is up sometimes but it is also random. 

There is no difference on the schematic of the PHY device used in both cards. In processor section following are the differences between card1 and card2 : 

CARD 1 
GPIO1_12 Pulled up via 10K resistor to 3.3 V 
GPIO1_13 Floating connected to a level translator device 
GPIO1_14 Pulled up via 10K resistor to 3.3 V 
GPIO1_15 Floating 

CARD 2 
GPIO1_12 Pulled up via 10K resistor to 3.3 V and connected to a level translator device 
GPIO1_13 connected to a level translator device 
GPIO1_14 Pulled up via 10K resistor to 3.3 V and connected to a level translator device 
GPIO1_15 connected to a level translator device 
Attached is the relevant schematic section for your reference. 

Note : In card 1 also this interface was not working earlier. Issue was resolved by replacing the bus-hold latch and buffer devices used at the local bus interface with the transparent latch and buffer devices. 

Kindly guide.

Labels (1)
Tags (1)
0 Kudos
5 Replies

650 Views
ufedor
NXP Employee
NXP Employee

It is required to check POR level of the GPIO1_15.

0 Kudos

650 Views
rinkutakkar
Contributor I

Hi,

Thanks for your reply.

We have checked voltage level at GPIO1_15. This is not powered down during the boot up of processor or to be precise before the deassertion of hreset signal by the cpld.

Thanks and Regards

Rinku

0 Kudos

650 Views
ufedor
NXP Employee
NXP Employee

> This is not powered down

What does it mean?

0 Kudos

650 Views
rinkutakkar
Contributor I

Voltage level at GPIO1_15 is 3.3 V during POR

0 Kudos

651 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> We have two different assembly options for the card with only a slight difference

It is needed to place both boards back-to-back and check POR behaviour of all configuration signals and signals explicitly mentioned in the notes after the Table 1. P1022 pinout listing in the P1022 HS.

0 Kudos