Reg.batch flush or clear of total per process mm context.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reg.batch flush or clear of total per process mm context.

690 Views
vasanthsri
Contributor III

Hi All,

Processor      : P4040

Linux             : 2.6.34

We have an application in which,  I observed certain operations (yet to be identified, mostly can think of tlb flush) is broadcast through "smp_call_function_many" procedure. I can see this procedure top in overhead which is captured by all the linux profilers. This application monitors changes in the memory through per process flag (something like "page modified ?") and in a given interval(less than a minute) this flag is cleared and respective mm/TLB page is flushed using tlb_page* .

This page flush was previously achieved using batch flush (one call to flush out the required things) and now it is not possible as because current kernel is of 32 bit version. I have tried a few things as below and didn't see any -new- changes as in happening (maybe the observed behavior (mentioned below) is expected)

- This application is allowed to run on only one core (affined) though we have 4 cores, so tried to make the flush local (local_tlb_*) with an assumption that no broadcast will happen and smp_call* can be avoided , but with new change (flush local) also not observed any difference in behavior

- Attempted to drop/flush the whole process context using flush_tlb_mm* with an assumption in this processor we can do per process TLB invalidation, but this didn't work rather resulted in exception

Along with "smp_call*" function "doorbell_message*" also one of the high runners which is incurring high overhead in my real time system .

Queries:

- Is it right, doing the flush of whole mm context when the process is healthily running

- Any alternative or similar like "batch flush" available for software maintained TLB's

- Is the "doorbell_message_" procedure call expected to happen when we have IPC between two processes running on different core ? or it has something to do with coherency stuff

Any other pointers on this regard will be helpful.

Thanks in Advance.

Labels (1)
0 Kudos
1 Reply

395 Views
vasanthsri
Contributor III

I got few clarification for the the first query "Is it right, doing the flush of whole mm context when the process is healthily running" from Kernel documentation by David.S.Miller. Thx.

Could someone provide view/pointers on remaining queries ? Thanks.

0 Kudos