QorIQ GPIO Input Buffer Enable register support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QorIQ GPIO Input Buffer Enable register support

2,597 次查看
robwestfall
Contributor II

In the Rev1 version of the T1040 Reference manual, the GPIO block got a new register - The "GPIO Input Buffer Enable Register (GPIOx_GPIBE)".  This was not in the older RevE manual.  The manual says this:

     The GPIO Input Buffer Enable register is used to control the input enable of each

     individual GPIO port. When an individual GPIO port’s direction is set to input

     (GPIO_GPDIR[DRn=0]), the associated input enable must be set (GPIOxGPIE[IEn]=1)

     to propagate the port value to the GPIO Data Register. When a port’s input enable is

     disabled, the port value does not propagate to the GPIO Data Register.

What CPU version was this implemented in? And what happens if I don't set them.  The documentation says that a value of zero makes the port disabled, and the reset value for the register is all zero's, meaning all inputs are disabled.

We are building a new CPU board that uses the T1042 cpu, and I'm confused about what happens here.  I am working off the T1040RDB, but it doesn't actually use any GPIO so it doesn't help me.

The latest UBoot software does not have this register in their register mapping headers.

Thanks,

Rob Westfall

Xerox Corporation

标签 (1)
0 项奖励
回复
4 回复数

2,271 次查看
ufedor
NXP Employee
NXP Employee

This is a documentation issue.

The section "22.4.7 GPIO Input Buffer Enable Register (GPIOx_GPIBE)" has to be discarded.

0 项奖励
回复

2,271 次查看
robwestfall
Contributor II

Is there an ERRATA doc for the QorIQ T1040 Reference Manual?

0 项奖励
回复

2,271 次查看
ufedor
NXP Employee
NXP Employee

This is a document generation issue which will be fixed in the next RM revision.

0 项奖励
回复

2,271 次查看
robwestfall
Contributor II

Any idea when the new version will be released?

0 项奖励
回复